Interface is highly experienced in working with organizations in the energy industry, both traditional and alternative, supplying force measurement solutions. We understand the unique requirements of green energy and have developed a widening line of products uniquely suited for these innovations. We’ve recently worked with multiple types of components for electric vehicles including batteries, engines and more, as well as with alternative energy sources like wind, solar, and hydrogen power. Interface brings the accuracy and reliability, in addition to having an expert engineering team that can quickly develop customized solutions. Interface solutions are cost effective and can often end up saving critical dollars in the long run. Take for example a recent case study we developed in which we outlined our role in harnessing hydrogen power using an electrolyzer. In this case, force sensors were used to significantly reduce downtown by creating an automated monitoring system that replaced regularly scheduled maintenance that was often unneeded but caused downtimes. And with that process came significant losses in energy and money. Interface helped to create an autonomous monitoring system that reduced downtime and ultimately estimated the customer would break even on their investment on the force monitoring system in one year.